Mouser Now Stocking NXP's MPC5777C Power Architecture MCU for Industrial and Automotive Engine Management
June 18, 2019 - Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking MPC5777C Power Architecture® microcontroller from NXP Semiconductors. Boasting three dual-issue, 32-bit CPU core complexes, the high-performance microcontroller supports demanding automotive and industrial engine management applications such as electric DC motor control, aerospace engines, and Ethernet and CAN FD connectivity, plus automotive applications that require compliance with SIL-1 and ASIL-D functional safety requirements.
The NXP MPC5777C Power Architecture microcontroller, available from Mouser Electronics, features two independent Power Architecture z7 cores offering up to 300 MHz operation, as well as a single z7 core operating in lockstep with one of the main computational cores. The two main cores offer signal processing extension instruction support for digital signal processing, as well as 16 Kbytes of I-cache and 16 Kbytes of D-cache. The microcontroller offers 8 Mbytes of on-chip flash memory, in addition to 512 Kbytes of on-chip general purpose RAM (including 64 Kbytes of standby RAM).
The device's two enhanced queued analog-to-digital converter (eQADC) modules provide support for 70 analog input pins, which can be expanded to 182 inputs using off-chip mutiplexers. The highly secure MPC5777C microcontroller includes on-chip security encryption protection using a tamper detection module and cryptographic services engine for tamper-proofing.
The NXP MPC5777C Power Architecture microcontroller is supported by the MPC5777C-DEVB development board, which enables the development of both hardware and software for applications such as battery management systems, traction motor control, and internal combustion engines and transmissions. The versatile development board includes an MPC5777C microcontroller together with MC33FS6520LAE System Basis Chip (SBC) and the TJA1100 and TJA1145T/FD Ethernet and CAN FD PHY transceivers.
To learn more about the NXP MPC5777C Power Architecture microcontroller, visit www.mouser.com/nxp-mpc5777c-mcu.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 750 manufacturers. Mouser offers 25 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in more than 220 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com