Mouser Electronics Now Stocking Dialog's Ultra-Small DA14531 SmartBond TINY SoC, Ideal for Medical Disposables
January 14, 2020 - Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the DA14531 SmartBond TINY system-on-chip (SoC) from Dialog Semiconductor. The low-power, cost-effective DA14531 is the industry's smallest and most power-efficient Bluetooth® 5.1 SoC, enabling new classes of Internet of Things (IoT) devices, including the growing market for connected medical products.
As an authorized distributor, Mouser Electronics is focused on the rapid introduction of new products and technologies, giving customers an edge and helping speed time to market. Over 800 semiconductor and electronic component manufacturers count on Mouser to help them introduce their products into the global marketplace. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each manufacturer.
The Dialog DA14531 SmartBond TINY SoC, available from Mouser Electronics, achieves a low system cost through a high level of integration. The SoC is based on an Arm® Cortex®-M0+ microcontroller with a complete set of analog and digital peripherals, and incorporates a 2.4 GHz transceiver in a minuscule form factor of just 2.0 × 1.7 mm. By adding just six external passives, a crystal oscillator, and power source, designers can build a complete Bluetooth Low Energy system for applications such as asset tracking, RFID tags, beacons, wearables, medical, and automotive applications.
Mouser also stocks the DA14531 SmartBond TINY Development Kits in Pro and USB versions. The DA14531 Development Kit Pro includes a Bluetooth Low Energy motherboard, daughterboard with the DA14531 SoC, and a mini-USB cable. The kit's extensive features include two mikroBUS header interfaces, Arduino Uno compatibility, and onboard 2-Mbit SPI data flash. The DA14531 Development Kit Pro allows users to perform RF measurements using an embedded printed antenna and SMA connector capability. The DA14531 Development Kit USB is a small, portable USB board with Bluetooth Low Energy technology, one mikroBUS connector, 2 Mbits of SPI flash, and an onboard DA14531 SoC.
To learn more about the Dialog DA14531 SmartBond TINY SoC, visit https://www.mouser.com/new/dialog-semiconductor/dialog-da14531-smartbond-tiny/. For more information about the development kits, go to https://www.mouser.com/new/dialog-semiconductor/dialog-da14531-dev-kit-pro/.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 800 manufacturers. Mouser offers 27 support locations around the world to provide best-in-class customer service and ships globally to over 630,000 customers in more than 223 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Dialog Semiconductor
Dialog Semiconductor creates highly integrated, mixed-signal integrated circuits (ICs), optimized for personal portable, low-energy short-range wireless, LED solid-state lighting and automotive applications. The company provides flexible and dynamic support, world-class innovation and the assurance of dealing with an established business partner.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com